Toshiba USA
Toshiba USA   Toshiba Americas
 
Search:  
Toshiba Storage Device Division
Storage Solutions
External Hard Drives
Enterprise Hard Drives
PC & Notebook Hard Drives
Specialty Products
Services & Support
Toshiba Drives
Fujitsu Drives
Company
Overview
Facts
Heritage
Environment
Social Responsibility
Global Storage Sites
Contacts
News
Trends & Technology
Storage Solutions  1.8-inch Hard Disk Drives  MKxx29GSG Series
MKxx29GSG Series:StorageSolutions/1.8-inchHardDiskDrives/MKxx29GSGSeries
 
MKxx29GSG Series Hard Disk Drive
120 / 160 / 250GB*
1.8-Inch / 5,400 RPM / SATA
MKxx29GSG
MKxx29GSG Series Data Sheet

Tiny in size but big in capacity, the MKxx29GSG is the industry’s first one-quarter terabyte, 1.8-inch hard disk drive.  The MKxx29GSG is Toshiba’s top-of-the-line 1.8-inch drive series which offers high capacity and fast performance for ultra-light, compact, extra-rugged and portable computing applications.  Coupling capacity with performance, the 250, 160 and 120GB models are equipped with a 5400 RPM rotational speed and 3 Gigabits per second Serial ATA interface using the Micro-SATA connector.  The MKxx29GSG products have passed testing by the Serial ATA International Organization (SATA-IO) for SATA interoperability. 

Toshiba’s vision for high-capacity, small form factor storage has helped the company maintain its number one position in the 1.8-inch market since the first drive shipped in 2000.  Toshiba’s 1.8-inch hard disk drives are used in some of the world’s most popular products, some of which have become common household names. 

Winner of the Storage Visions TM 2009
Visionary Products Consumer Home Storage Award

 
Key Features Specifications Support 
  • 1.8-inch Footprint
  • Up To A Quarter-Terabyte (250 GB*) Of Capacity
  • 5400 RPM Spin Speed
  • Serial ATA 2.6 / ATA-8 Interface
  • Micro-SATA Connector
  • 8MB Cache Buffer
 
*One Gigabyte (1 GB) means 109 = 1,000,000,000 bytes using powers of 10. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1 GB = 230 = 1,073,741,824 bytes, and therefore shows less storage capacity. Available storage capacity will also be less if the computer includes one or more pre-installed operating systems, pre-installed software applications, or media content. Actual formatted capacity may vary.


Subject to Change: While Toshiba has made every effort at the time of publication to ensure the accuracy of the information provided herein, product specifications, configurations, prices, system/component/options availability are all subject to change without notice.