Toshiba USA
Toshiba USA   Toshiba Americas
 
Search:  
Toshiba Storage Device Division
Storage Solutions
External Hard Drives
Enterprise Hard Drives
PC & Notebook Hard Drives
Specialty Products
Services & Support
Toshiba Drives
Fujitsu Drives
Company
Overview
Facts
Heritage
Environment
Social Responsibility
Global Storage Sites
Contacts
News
Trends & Technology
Services & Support  Jumper Settings
Jumper Settings:ServicesSupport/JumperSettings
 
  Jumper Settings
 
Optical Disk Drives
Toshiba's half-height CD-ROMs, CD-RW/DVD-ROM, DVD-ROMs and DVD-RAMs have jumper settings that may need to be changed in order for your drive to work properly. (The slim-line CD-ROMs and DVD-ROMs do not have jumpers.)
 
ATAPI CD-ROM, CD-RW/DVD-ROM,DVD-ROM
SCSI CD-ROM & DVD-ROM
SCSI DVD-RAM
Hard Disk Drives
Toshiba's 2.5" hard disk drives can be configured as either master or slave units. Master configuration is used for all single drive applications, and master or slave configuration (only one of each per port) is used for two drive applications. Use the information in the following tables for information on how to set Master/Slave jumpers.
Jumper settings for PATA drives