Toshiba USA
Toshiba USA   Toshiba Americas
 
Search:  
Toshiba Storage Device Division
Storage Solutions
External Hard Drives
Enterprise Hard Drives
PC & Notebook Hard Drives
Specialty Products
Services & Support
Toshiba Drives
Fujitsu Drives
Company
Overview
Facts
Heritage
Environment
Social Responsibility
Global Storage Sites
Contacts
News
Trends & Technology
Services & Support  Device Drivers
Device Drivers:ServicesSupport/DeviceDrivers
 
  Device Drivers
 
ATAPI CD-ROM and DVD Drivers
Toshiba's CD-ROM and DVD-ROM drives do not require any unique device drivers for Windows '95/'98/2000/XP/NT.
After installing your drive and re-booting, your system should recognize your CD-ROM or DVD-ROM. Win '95/'98/2000/XP/NT Operating Systems support all Toshiba ATAPI CD-ROM and DVD-ROM drives natively.
DOS/Windows 3.x Device Drivers
This device driver is to be used with DOS/Windows 3.x operating systems. Do not use this driver with Windows '95, Windows '98, XP or Windows 2000 unless you are going to use your system in the REAL or MS-DOS Modes. Device drivers for Windows '95, Windows '98, Windows 2000, XP, OS/2, and NT operating systems are provided with the installation or setup software of each operating system.
DOS ATAPI Interface Driver
If you prefer using DOS click the link below to download a MS-DOS ATAPI interface driver.
atapi.exe
SCSI CD-ROM and DVD Drivers
SCSI interface drivers are written for the SCSI card you are using in your system, by the SCSI card manufacturer. They are not specific to your Toshiba drive and are not provided by Toshiba. If during installation Windows can not find the correct SCSI software driver for your SCSI card and you do not have the software driver that came with your SCSI card, contact your SCSI host adapter manufacturer.
Adaptec SCSI Drivers
LSI Logic (Symbios) SCSI Drivers
DVD Viewing Software
Toshibas DVD drives require a third party software to be installed in your system to enable you to view DVD movies. If you purchased your drive as part of a kit, the software may have been included. The links below will provide some possible solutions should you not have this type of software.
Nero6 (Toshiba recommends)
Toshiba does not recommend nor endorse any of the following manufacturers software products. Software names are provided only as a courtesy to our customers. Please check with the software manufacturer to assure that their software supports your drive model.
DirectDVD
Cyberlink PowerDVD
WinDVD
Media Burning Software
Toshiba's recordable drives require third party software to be installed in your system to enable you to burn media. If you purchased your drive as part of a kit, the software may have been included. The link below will provide some possible solutions should you not have this type of software.
Nero6 (Toshiba recommends)
Toshiba does not recommend nor endorse any of the following manufactures software products. Software names are provided only as a courtesy to our customers. Please check with the software manufacturer to assure that their software supports your drive model.
NTI CD & DVD Maker
Gear DVD & CD-RW
Roxio Toast (Macintosh)
Easy CD Creator
Stomp Clinkn Burn Pro